ECAT.POSLOOPTIME

Description

This parameter allows viewing and recording of the Distributed Clock (DC) time of the first position loop after the Phase-Locked Loop (PLL) reference. This ideally happens after ECAT.RXDONETIME for proper control. If it occurs before, then either the SM2 offset should be increased in the master or ECAT.PLLOFFSET can be increased in the drive.

Context

See Synchronization.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read Only

Units

ns

Range

0 to 4,294,967,295 ns

Default Value

N/A

Data Type

Integer
See Also ECAT.RXIRQTIME, ECAT.RXDONETIME, ECAT.TXDONETIME, ECAT.SYNC0TIME

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT variants: AKD2G-SPE

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ECAT.POSLOOPTIME

4300h

04h

Unsigned32

-

-

Read only

Yes